MFG Tool stops in loading u-boot

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MFG Tool stops in loading u-boot

1,466件の閲覧回数
shanmugamsundar
Contributor IV

Hi all,

I am using a imx6dual processor for our customized board, in that we are using SPI 4 for nor flash, for that i have changed the spi form 0 to 4 in the files mx6q_sabrelite_android.h and mx6q_sabrelite.c , but when i tried to load the u-boot.bin from mfg tool, it stops after the jumping to os  and stays in loading u-boot, screen

Note:

Plz check is this configuration is correct and plz tell me if i missed any thing and is it possible to flash u-boot in emmc for a dual processor?

CHANGES I HAVE DONE IN THE FILES

All the mux configuration are correct i have check with our schematic

mx6q_sabrelite.c

s32 spi_get_cfg(struct imx_spi_dev_t *dev) //OVIYA ADDED

{

        switch (dev->slave.cs) {

        case 0:

                /*    PMIC

                dev->base = ECSPI1_BASE_ADDR;

                dev->freq = 25000000;

                dev->ss_pol = IMX_SPI_ACTIVE_HIGH;

                dev->ss = 0;

                dev->fifo_sz = 64 * 4;

                dev->us_delay = 0;

             break;   */

      /* SPI-NOR */

             dev->base = ECSPI4_BASE_ADDR;

                dev->freq = 25000000;

           dev->ss_pol = IMX_SPI_ACTIVE_LOW;

                dev->ss = 0;

                dev->fifo_sz = 64 * 4;

                dev->us_delay = 0;

                break;

        default:

                printf("Invalid Bus ID!\n");

        }

        return 0;

}

void spi_io_init(struct imx_spi_dev_t *dev) //OVIYA ADDED

{

        switch (dev->base) {

        case ECSPI4_BASE_ADDR:

                /* SCLK */

                mxc_iomux_v3_setup_pad(MX6Q_PAD_EIM_D21__ECSPI4_SCLK);

                /* MISO */

                mxc_iomux_v3_setup_pad(MX6Q_PAD_EIM_D22__ECSPI4_MISO);

                /* MOSI */

                mxc_iomux_v3_setup_pad(MX6Q_PAD_EIM_D28__ECSPI4_MOSI);

                if (dev->ss == 0)

                        mxc_iomux_v3_setup_pad(MX6Q_PAD_EIM_D20__ECSPI4_SS0);

                break;

        case ECSPI2_BASE_ADDR:

        case ECSPI3_BASE_ADDR:

                /* ecspi2-3 fall through */

                break;

        default:

                break;

        }

}

mx6q_sabrelite_android.h

#ifdef CONFIG_CMD_SF

        #define CONFIG_FSL_SF           4

        #define CONFIG_SPI_FLASH_IMX_SST        1

        #define CONFIG_SPI_FLASH_CS     0

        #define CONFIG_IMX_ECSPI

        #define IMX_CSPI_VER_2_3        1

        #define MAX_SPI_BYTES           (64 * 4)

#endif

#elif defined(CONFIG_FSL_ENV_IN_SF)    

        #define CONFIG_ENV_IS_IN_SPI_FLASH      4

        #define CONFIG_ENV_SPI_CS               0

        #define CONFIG_ENV_OFFSET       (768 * 1024)

ラベル(3)
タグ(1)
0 件の賞賛
返信
0 返答(返信)