MQX vectorrom Location

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MQX vectorrom Location

Jump to solution
1,916 Views
Mike_d
Contributor IV

Hi,

I've been trying to get an MQX application to run with a modified vectorrom entry in the linker file so that I can clear space for a bootloader.  MQX will not run unless the vectorrom is set to address 0x00000000 regardless of whether I specify to use vectors in RAM or not. Can you tell me what I'm missing here?  I've referenced AN4370, AN4367 and AN4379.

Thanks,

-Mike

Tags (2)
0 Kudos
Reply
1 Solution
1,601 Views
DavidS
NXP Employee
NXP Employee

In addition to Kojto's reply please review the following post:

https://community.freescale.com/message/305284#305284

Regards,

David

View solution in original post

0 Kudos
Reply
2 Replies
1,601 Views
c0170
Senior Contributor III

Hello Michale del Busto,

what's your target MCU? Kinetis - Cortex M4? What do you mean it does not run? Some details could have been provided :smileywink:  What did you attempt to do with your linker command file and an application?

Regards,

MartinK

1,602 Views
DavidS
NXP Employee
NXP Employee

In addition to Kojto's reply please review the following post:

https://community.freescale.com/message/305284#305284

Regards,

David

0 Kudos
Reply