MQX vectorrom Location

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MQX vectorrom Location

ソリューションへジャンプ
1,969件の閲覧回数
Mike_d
Contributor IV

Hi,

I've been trying to get an MQX application to run with a modified vectorrom entry in the linker file so that I can clear space for a bootloader.  MQX will not run unless the vectorrom is set to address 0x00000000 regardless of whether I specify to use vectors in RAM or not. Can you tell me what I'm missing here?  I've referenced AN4370, AN4367 and AN4379.

Thanks,

-Mike

タグ(2)
0 件の賞賛
返信
1 解決策
1,654件の閲覧回数
DavidS
NXP Employee
NXP Employee

In addition to Kojto's reply please review the following post:

https://community.freescale.com/message/305284#305284

Regards,

David

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,654件の閲覧回数
c0170
Senior Contributor III

Hello Michale del Busto,

what's your target MCU? Kinetis - Cortex M4? What do you mean it does not run? Some details could have been provided :smileywink:  What did you attempt to do with your linker command file and an application?

Regards,

MartinK

1,655件の閲覧回数
DavidS
NXP Employee
NXP Employee

In addition to Kojto's reply please review the following post:

https://community.freescale.com/message/305284#305284

Regards,

David

0 件の賞賛
返信