Sorry my misstake, I was looking at an existing schematic and there it is the SD4_CLK which is muxed with NANDF_WE and the SD4_CMD is in pinunion with NANDF_RE.
Please use the pin-muxer tool from freescale to plan the pins (the rawnand section provides all pin-options for the nand).
After checking, it looks like the we/re signals are ONLY available on E16/B17
The hard way is to understand the iomux section in the reference manual (table 4.1 in chapter 4) and pick the best for your routing. (search for rawnand and rdn or wdn )