Yocto error with populate_sdk and devtool with tee.bin

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Yocto error with populate_sdk and devtool with tee.bin

234 Views
mlopez_airfal
Contributor I

Hi,

I've got a Yocto distribution installed for an i.mx8M PLUS processor board.

To be able to compile my own programs, to create the toolchain I use:

bitbake core-image-minimal -c populate_sdk

Then I want to make changes to linux image (DTS definition), so I've installed devtool with:

devtool modify virtual/kernel

So I create the linux image after making changes with:

devtool build linux-imx

This works ok, but If I want now to install new recipes to Yocto, I make again:

bitbake core-image-minimal -c populate_sdk

And now I get an error related to tee.bin:

ERROR: imx-boot-1.0-r0 do_compile: ExecutionError('/home/yo/Atenea/Yocto/IBR215-yocto5.0-bsp-20241101/ibr215/tmp/work/imx8mpevk-poky-linux/imx-boot/1.0/temp/run.do_compile.4739', 1, None, None)
ERROR: Logfile of failure stored in: /home/yo/Atenea/Yocto/IBR215-yocto5.0-bsp-20241101/ibr215/tmp/work/imx8mpevk-poky-linux/imx-boot/1.0/temp/log.do_compile.4739
Log data follows:
| DEBUG: Executing shell function do_compile
| cp: cannot stat '/home/yo/Atenea/Yocto/IBR215-yocto5.0-bsp-20241101/ibr215/workspace/deploy/images/tee.bin': No such file or directory

What am I doing wrong?

Regards

0 Kudos
Reply
0 Replies