USB Camera Interface with iMX6 SABRE

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

USB Camera Interface with iMX6 SABRE

1,864 Views
i_ashok_s
Contributor I

Hi,

I am using iMX6 SABRELITE for my application development. I need to interface usb camera to the board. In a simple way, i need to test it using vlc installed on board. I can see the camera module detected as 'video4' in '/dev/video*'. Once i run the vlc, it shows....

[006ddb58] main libvlc: Running vlc with the default interface. Use 'cvlc' to use vlc without interface.
[0073f9f8] main playlist: playlist is empty

and nothing happens.

Please suggest! 

Thanks.

0 Kudos
Reply
1 Reply

1,803 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Hi,

    The log remind you "Use 'cvlc' to use vlc without interface"

    it means you should use cvlc command, not vlc.

Have a nice day!

B.R,

weidong

0 Kudos
Reply