U-Boot build issue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

U-Boot build issue

2,326件の閲覧回数
atian
Contributor I

Hi, we need to build the U-boot in standalone environment for 8MMINILPD4-EVK , but it's not working properly.. Please advise the solution for build the U-boot and solve our problem.

①Version:
Ubuntu 16.04 LTS
imx-yocto-L4.14.98_2.0.0_ga
gcc (Ubuntu 5.4.0-6ubuntu1~16.04.12) 5.4.0 20160609
sdk:DISTRO=fsl-imx-fb MACHINE=imx8mmevk bitbake core-image-minimal -c populate_sdk
defconfig:imx8mm_evk_defconfig
②Reference documents:i.MX_Porting_GuideL4.14.98-2.0.0_ga.pdf
③Error message:
gcc: error: unrecognized command line option ‘-mgeneral-regs-only’

0 件の賞賛
返信
1 返信

2,292件の閲覧回数
Forlinx
Contributor I

we have i.MX8M Mini based EVK and SoM with supporting of Linux4.14.78 with QT5.10, and also supporting of Android9.0, if you need help, you can send us email to grace@forlinx.com

0 件の賞賛
返信