IMX8QXP will not flash new image

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

IMX8QXP will not flash new image

跳至解决方案
2,414 次查看
lrd_qa
Contributor I

I recently flashed an Andriod10 image to my IMX8QXP-mek board. The image works fine but when I try to flash a new image I get the following:

./uuu_imx_android_flash.sh -f imx8qxp  

dtbo is supported 

dual slot is supported 

dynamic parttition is supported 

generate lines to flash u-boot-imx8qxp.imx to the partition of bootloader0

generate lines to flash partition-table.img to the partition of gpt

generate lines to flash dtbo-imx8qxp.img to the partition of dtbo_a 

generate lines to flash boot.img to the partition of boot_a

generate lines to flash vbmeta-imx8qxp.img to the partition of vbmeta_a

generate lines to flash dtbo-imx8qxp.img to the partition of dtbo_b

generate lines to flash boot.img to the partition of boot_b

generate lines to flash vbmeta-imx8qxp.img to the partition of vbmeta_b

Invalid sparse file format at header

Invalid input image file. 

The board will allow me to flash the same image over and over but nothing new. Tried to erase userdata using fastboot but still could not re-flash board.

0 项奖励
回复
1 解答
2,399 次查看
lrd_qa
Contributor I

Problem solved. When I extracted the downloaded image files, the files were empty which obviously failed to flash onto my board.

在原帖中查看解决方案

0 项奖励
回复
1 回复
2,400 次查看
lrd_qa
Contributor I

Problem solved. When I extracted the downloaded image files, the files were empty which obviously failed to flash onto my board.

0 项奖励
回复