How get 3 camera images at the same time?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How get 3 camera images at the same time?

1,636件の閲覧回数
JeanChao
Contributor I

I want to get  the images from 3 cameras for further immaging process through processor.

1. Is there any way to get continuous images of 3 cameras at the same time?
2. How to synchronize? 

 

Platefrom: i.MX8M

OS: Linux

0 件の賞賛
返信
2 返答(返信)

1,621件の閲覧回数
weidong_sun
NXP TechSupport
NXP TechSupport

Hi,

  iMX8MQ supports 2 MIPI CSI-2 port, so you can connect 2 cameras.

  No.3 camera should be connected to USB port.

  so you cameras will be :   2 of them should be MIPI CSI-2 interface, 1 of them is USB interface.

 

Hope the information is helpful to you.

Have a nice day!

B.R

weidong

0 件の賞賛
返信

1,619件の閲覧回数
JeanChao
Contributor I

Hi Weidong,

Thanks for your reply.

Yes, I want to connect 2 cameras to mipi interface, and another one through usb using CYUSB306X. And, our concern is how to align image from 3 different cameras as well as their timing.

That will be very helpful if you can share any idea of how to synchronize them.

Thanks,

Jean

0 件の賞賛
返信