How get 3 camera images at the same time?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How get 3 camera images at the same time?

2,179 Views
JeanChao
Contributor I

I want to get  the images from 3 cameras for further immaging process through processor.

1. Is there any way to get continuous images of 3 cameras at the same time?
2. How to synchronize? 

 

Platefrom: i.MX8M

OS: Linux

0 Kudos
Reply
2 Replies

2,164 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Hi,

  iMX8MQ supports 2 MIPI CSI-2 port, so you can connect 2 cameras.

  No.3 camera should be connected to USB port.

  so you cameras will be :   2 of them should be MIPI CSI-2 interface, 1 of them is USB interface.

 

Hope the information is helpful to you.

Have a nice day!

B.R

weidong

0 Kudos
Reply

2,162 Views
JeanChao
Contributor I

Hi Weidong,

Thanks for your reply.

Yes, I want to connect 2 cameras to mipi interface, and another one through usb using CYUSB306X. And, our concern is how to align image from 3 different cameras as well as their timing.

That will be very helpful if you can share any idea of how to synchronize them.

Thanks,

Jean

0 Kudos
Reply