i.MX解决方案知识库

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i.MX Solutions Knowledge Base

标签

讨论

排序依据:
The board Added by Pierantonio Tabaro on February 3, 2012 at 5:04am   One prototype of our product based on i.MX28
查看全文
Trisendo 2D/3D Video Board Added by Leon Woestenberg on February 19, 2012 at 9:56am   The Trisendo Video Board mounts directly onto the i.MX53QSB.   Using FPGA video processing the reference design demonstrates 2D+Z to 3D rendering for 3D displays that do not require 3D glasses.  
查看全文
iMX233-QBIT Added by Renato Torres Tovar on February 4, 2011 at 1:22am    
查看全文
http://www.youtube.com/watch?v=78cdXXDXb6E&feature=player_embedded   Published on Aug 1, 2012 by DeviceSolutionsLtd The Opal i.MX53 CPU Module integrates a Freescale i.MX53 processor, memory and power supply components. Using Opal reduces development time and cost for companies developing high-end industrial, medical and automotive devices. http://devicesolutions.net/OpalModule Category: Science & Technology License: Standard YouTube License  
查看全文
Added by Marsha Chang on March 16, 2011 at 11:16am
查看全文
img-0009-ptx Added by Robert Schwebel on November 10, 2010 at 6:46pm   Showing mainline Linux 2.6.26 on MX23, MX27, MX28 and MX35 at the Pengutronix booth
查看全文
Derald Woods Added by Derald Woods on January 16, 2012 at 9:00pm    
查看全文
SBC+TVP_notes Added by Lautaro Carmona on September 26, 2011 at 10:49am Here is our hardware framework. We are using BlueTechnix Single Board Computer SBC-i.MX51 with our TVIN board with TVP5147 TV encoder.   We connect them together through an 80-pin connector, which includes:   CSI1.Data[0:9] CSI1.PIXCLK CSI1.HS CSI1.VS CSI1.MCLK CSI1.PWDN I2C_SDA I2C_SCL  
查看全文
http://www.youtube.com/watch?v=Hqd38STiaa0&feature=player_embedded   Uploaded by ericymiao on Dec 29, 2011 Demo of LVDS and touch screen on SabreLite Category: People & Blogs License: Standard YouTube License  
查看全文
iWave’s i.MX6 Qseven System on Module has been incorporated into the Golf Cart Guide System which is used to monitor the cart position, delay while supplementing the cart position, to identify the members with the player list in the clubhouse. The design also includes ensuring safety of golfers by giving warning messages during lightning, fog etc. iWave’s i.MX6 Qseven module was seamlessly integrated with customer carrier card. Given iWave’s design Quality and Technical Support client could easily adapt iWave’s SOM into their design. Key technology iWave has worked on this solution: Freescale i.MX6x Solo core Qseven SOM (extended commercial grade) ARM Cortex A9 core at 800MHz OS: Windows Embedded Compact 7 High brightness LCD display Touch panel AC’97 Audio Key input GPS WiFi SDIO interface USB memory iWave’s unique ability to provide qseven module and BSP support under one roof helped the client to shorten the product development life cycle and achieve quick time to market. iWave’s i.MX6 Qseven SOM iW-RainboW-G15M-Q7 has gained worldwide popularity due to the ease of usage for diverse range of applications. Along with this, availability of the iW-RainboW-G15D-Q7 (i.MX6 development/ i.MX6 evaluation board) and iWave’s in-house software BSP support for i.MX6 helps clients to validate the end application quickly and achieve short product development life cycle and quick time to market. For further information please write to mktg@iwavesystems.com or visit www.iwavesystems.com
查看全文
iWave has now enabled 2GB RAM support for the iW-RainboW-G15M-Q7, the i.MX6 Quad, Dual & Dual Lite Qseven SOMs. The 2GB RAM support allows customers to run graphics and multimedia rich applications more seamlessly. The 2GB RAM supported Qseven SOM configuration is available with minimum order quantity of 500pcs. iWave also can support 4GB RAM on specific requests. For more details contact mktg@iwavesystems.com
查看全文
http://www.youtube.com/watch?feature=player_embedded&v=yMiIxDdUskQ   Uploaded by manish590 on Jul 9, 2010 No description available. Category: Education License: Standard YouTube License  
查看全文
http://www.youtube.com/watch?v=PmHNecNguDM&feature=player_embedded   Uploaded by Charbax on Jun 21, 2011 Here is the board for now, they are going to launch the new Genesi i.MX53 based Laptops and Desktops around July or August, to provide more performance, using lower power and at lower cost. The current Genesi Efika MX i.MX51 based laptop is selling for $199, the Genesi i.MX51 Desktop is $129, they plan for the next generation i.MX53 based Laptop and Desktop to be sold for even cheaper. They are also working to combine their ARM based Laptop with the Pixel Qi screen as soon as it's mass produced. Category: Science & Technology License: Standard YouTube License  
查看全文
QBIT Running Linux - Matchbox Added by Renato Torres Tovar on January 7, 2012 at 8:58pm QBIT embedded system... I.MX23, 128LQFP    
查看全文
iMX53 Added by Ramona Maurer on November 13, 2011 at 8:43am DIMM module with i.MX53 on emtrion base module LOTHRON, also available as Developer Kit  
查看全文
Added by Renato Frias on May 19, 2010 at 4:29pm     http://www.youtube.com/watch?feature=player_embedded&v=kpIkE1LQCsg   Uploaded by renatofrias55 on May 19, 2010 Freescale's i.MX25 PDK booting from SD card with a splash screen bitmap loaded from SD also on u-Boot start up. The LCD blinks when Linux takes over the Framebuffer. For more details, see: http://www.imxdev.org/wiki/index.php?title=I.MX25_PDK_U-boot_SplashScreen Category: Science & Technology License: Standard YouTube License  
查看全文
The i.MX53 General Market Launch at Embedded World Added by Marsha Chang on March 8, 2011 at 6:34pm The i.MX53 launch was successful at Embedded World in Nuremberg, Germany. We had many partners demoing i.MX53 solutions as well as the i.MX53 Quick Start board showing HD1080p video decode and the i.MX53 Tablet reference design (SABRE Platform for Tablets). For more information, visit www.freescale.com/imx53.  
查看全文
Dear,   Now we could use USB port for program downloading, do we have serial port download tools for i.mx6UL? For Jlink tools, now it could start running with Jlink, but after power off and power on, the target will not start. Do you have the image which could download to QSPI norflash by Jlink, and after power on, the target board could running.
查看全文
img-0008-fsl-ptx Added by Robert Schwebel on November 10, 2010 at 6:46pm   Pengutronix' Mainline Linux engineers demonstrate the brand new i.MX28.
查看全文