Support SDIO-UART 8987 on mek_8q

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Support SDIO-UART 8987 on mek_8q

Support SDIO-UART 8987 on mek_8q

Below are the patches to support SDIO-UART 8987 M2 module on mek_8q M2 port. After applying the patches, PCIe chip can't be recognized on M2 port. Revert the patches if want to use PCIe chip. Patches are from Andy Duan.

--- a/board/freescale/imx8qm_mek/imx8qm_mek.c
+++ b/board/freescale/imx8qm_mek/imx8qm_mek.c
@@ -373,6 +373,7 @@ int board_init(void)
#if defined(CONFIG_USB) && defined(CONFIG_USB_TCPC)
        setup_typec();
#endif
+       sc_pm_set_resource_power_mode(-1, SC_R_BOARD_R3, SC_PM_PW_MODE_ON);
#ifdef CONFIG_SNVS_SEC_SC_AUTO
        {
--- a/arch/arm64/boot/dts/freescale/imx8qm-mek.dts
+++ b/arch/arm64/boot/dts/freescale/imx8qm-mek.dts
@@ -151,6 +151,11 @@
 
  };
 
+ usdhc3_pwrseq: usdhc3_pwrseq {
+  compatible = "mmc-pwrseq-simple";
+  reset-gpios = <&lsio_gpio1 13 GPIO_ACTIVE_LOW>;
+ };
+
  epdev_on: fixedregulator@100 {
   compatible = "regulator-fixed";
   pinctrl-names = "default", "sleep";
@@ -159,8 +164,6 @@
   regulator-min-microvolt = <3300000>;
   regulator-max-microvolt = <3300000>;
   regulator-name = "epdev_on";
-  gpio = <&lsio_gpio1 13 0>;
-  enable-active-high;
  };
 
  reg_fec2_supply: fec2_nvcc {
@@ -1036,6 +1039,22 @@
  status = "okay";
 };
 
+&usdhc3 {
+        pinctrl-names = "default", "state_100mhz", "state_200mhz";
+        pinctrl-0 = <&pinctrl_usdhc3>,<&pinctrl_usdhc3_gpio>;
+        pinctrl-1 = <&pinctrl_usdhc3>,<&pinctrl_usdhc3_gpio>;
+        pinctrl-2 = <&pinctrl_usdhc3>,<&pinctrl_usdhc3_gpio>;
+        bus-width = <4>;
+ pinctrl-assert-gpios = <&lsio_gpio4 9 GPIO_ACTIVE_HIGH>;
+ pinctrl-assert-gpios = <&lsio_gpio4 10 GPIO_ACTIVE_HIGH>;
+ mmc-pwrseq = <&usdhc3_pwrseq>;
+ pm-ignore-notify;
+ keep-power-in-suspend;
+ non-removable;
+ cap-power-off-card;
+        status = "okay";
+};
+
 &i2c0 {
  #address-cells = <1>;
  #size-cells = <0>;
@@ -1540,7 +1559,6 @@
   fsl,pins = <
    IMX8QM_PCIE_CTRL0_WAKE_B_LSIO_GPIO4_IO28  0x04000021
    IMX8QM_PCIE_CTRL0_PERST_B_LSIO_GPIO4_IO29  0x06000021
-   IMX8QM_USDHC2_RESET_B_LSIO_GPIO4_IO09   0x06000021
   >;
  };
 
@@ -1618,7 +1636,26 @@
    IMX8QM_USDHC1_DATA1_CONN_USDHC1_DATA1   0x00000021
    IMX8QM_USDHC1_DATA2_CONN_USDHC1_DATA2   0x00000021
    IMX8QM_USDHC1_DATA3_CONN_USDHC1_DATA3   0x00000021
-   IMX8QM_USDHC1_VSELECT_CONN_USDHC1_VSELECT  0x00000021
+   IMX8QM_USDHC1_VSELECT_CONN_USDHC1_VSELECT               0x00000021
+  >;
+ };
+
+ pinctrl_usdhc3_gpio: usdhc3grpgpio {
+  fsl,pins = <
+   IMX8QM_USDHC2_VSELECT_LSIO_GPIO4_IO10   0x00000021
+   IMX8QM_LVDS1_I2C0_SDA_LSIO_GPIO1_IO13   0x06000021
+   IMX8QM_USDHC2_RESET_B_LSIO_GPIO4_IO09   0x06000021
+  >;
+ };
+
+ pinctrl_usdhc3: usdhc3grp {
+  fsl,pins = <
+   IMX8QM_USDHC2_CLK_CONN_USDHC2_CLK         0x06000041
+   IMX8QM_USDHC2_CMD_CONN_USDHC2_CMD         0x00000021
+   IMX8QM_USDHC2_DATA0_CONN_USDHC2_DATA0     0x00000021
+   IMX8QM_USDHC2_DATA1_CONN_USDHC2_DATA1     0x00000021
+   IMX8QM_USDHC2_DATA2_CONN_USDHC2_DATA2     0x00000021
+   IMX8QM_USDHC2_DATA3_CONN_USDHC2_DATA3     0x00000021
   >;
  };
 
@@ -1680,13 +1717,11 @@
 
  pinctrl_wlreg_on: wlregongrp{
   fsl,pins = <
-   IMX8QM_LVDS1_I2C0_SDA_LSIO_GPIO1_IO13  0x06000000
   >;
  };
 
  pinctrl_wlreg_on_sleep: wlregon_sleepgrp{
   fsl,pins = <
-   IMX8QM_LVDS1_I2C0_SDA_LSIO_GPIO1_IO13  0x07800000
   >;
  };
 
添付
評価なし
バージョン履歴
最終更新日:
‎07-15-2020 10:18 PM
更新者: