i.MX Security Features & Collateral

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX Security Features & Collateral

i.MX Security Features & Collateral

i.MX Trust.jpg


Topic

Link Comments

Secure Boot 

Secure Boot in AHAB enabled devices

Applies to i.MX 8/8X/8XLite Family of Application Processors

Extended to support i.MX 8ULP and i.MX 93 Family of Application Processors

Secure boot - step-by-step guides for both HAB and AHAB enabled devices

 

Secure Boot Automation -  Reference Design

 Please switch to the latest BSP version for the updated guides.

Security Reference Design - Yocto based Secure Boot automation

Documentation at IMXLUG: Chapter "Security Reference Design"

Secure Boot with i.MX 28 HAB Version 4

Applies to i.MX 28 Application Processor

Secure boot in HABv4 enabled devices

Applies to i.MX 6/7/8M Family of Application Processors

Encrypted Boot 

 

Encrypted boot App Note for HABv4 and CAAM enabled devices

Applies to i.MX 6/7/8M Family of Application Processors

Encrypted boot - step-by-step Guides for HAB enabled devices

Encrypted boot - step-by-step Guides for AHAB enabled devices

Link may not be updated with the latest BSP release. Please switch to the latest BSP or the required version.

Security Training


 

 


 

 


 

 


 

i.MX Security Training

Various Security Training Workshops on older BSP releases.  NDA customers will need to request access from NXP.

Secure Manufacturing Training

Manufacturing Protection: Provision Sensitive Material in an Unsecure Environment

Software Integrity and Data Confidentiality: Establishing Secure Boot and Chain of Trust on i.MX Pro...

This training explores the “Secure by Design” approach to software security for embedded systems using NXP i.MX processors - specifically, establishing secure boot and chain of trust 

Securing Embedded Linux Devices: Pitfalls to Avoid

This training session explores the proven best practices for designing and maintaining secure products, common security pitfalls & tips for hardening embedded Linux devices.

Linux Kernel Security: Overview of Security Features and Hardening

This training session explores how the Linux kernel's configuration can be strengthened to protect against security exploits.

Essential Security Considerations for Edge Applications

This training session introduces key features of embedded security, from secure boot and debug to lifecycle management.

Code Signing Tool

Latest Code Signing Tool

Code Signing Tool (CST) package with complete source code and documentation.

Using Code Signing Tool with Hardware Security Module

Hardware Security Module backend exposed to extend the usage of CST with external HSM

Using HSM mode for code signing in AHAB devices

Using HSM mode for code signing in HAB devices

 Offline HSM Code signing support for both HAB and AHAB based devices

Secure Provisioning Tool (SPSDK)

Latest SPSDK source code

SPSDK source code Github repository

Latest SPSDK documentation

SPSDK readthedocs documentation covering Build/Installation, API, user guide and examples

Supported MPU Devices
- i.MX 8 ULP

- i.MX 9 Family

 

Device specific examples :

- i.MX 8ULP AHAB with U-BOOT

- i.MX 95 AHAB with U-BOOT

- i.MX 93 signed and encrypted AHAB image

- i.MX 93 signed and encrypted AHAB image

etc..

Examples such as:

- secure boot/encrypted boot

- secure debug

- boot image build/deployment

- Key creation/management

EdgeLock Secure Enclave (ELE)

Security Beyond the Edge | EdgeLock Secure Enclave

 EdgeLock Secure EnclaveE API Reference Guide

UG10186 EdgeLock Secure Enclave i.MX93 A1 User Guide

UG10190 EdgeLock Secure Enclave i.MX95 B0 User Guide

UG10404 V2X Secure Enclave i.MX95 B0 User Guide 

The EdgeLock® Secure enclave is a preconfigured, self-managed and autonomous security subsystem that enables embedded developers to achieve their device security goals.

 

User guides Available through - Secure Resources

Secure Debug 

Secure Debug on devices with JTAG controller

Secure Debug on devices with JTAG controller and Authenticated Debug Module (ADM)

Applies to i.MX 6/7/8M Family of Application Processors

Applies to i.MX 8/8x Family of Application Processors

 
Secure Debug on ELE-AP based i.MX SoCs - New
 AN14579 applies to i.MX 9 Family of Application Processors (ELE-AP)

Extending the Root of Trust

HABv4 RVT guidelines and recommendations 

The HAB API allows the use of the HAB library to extend the root of trust and authenticate additional software images. This document describes system considerations when planning to make use of this API.

HAB Persistent memory 

HABv4 persistent memory address regions for various i.MX Application Processors

HAB persistent memory is used by HAB to store logs. The base address and size are provided for each processor.

OP-TEE


 

i.MX Porting Guide - Configuring OP-TEE chapter

Guide to OPTEE enablement on various i.MX devices can be requested for customers under NDA

Getting Started with OP-TEE on i.MX Processors

Webinar - Getting started with trusted execution environments (TEE) - OPTEE enablement on various i.MX devices 

Secure  Updates

Secure Over the Air Updates

Source Code 

______________________________

 

Enabling SWUpdate on i.MX 6ULL, i.MX 8M Mini & i.MX 93

______________________________ 

Secure Software Updates: Designing Ota Updates For Secure Embedded Linux Systems

Secure Over-the-Air Prototype for Linux Using CAAM and Mender or SWUpdate

______________________________

SWUpdate is a Linux Update agent to provide an efficient and safe way to update an embedded Linux system. SWUpdate supports local and OTA updates, & multiple update strategies

___________________________

Webinar on Field updates of the software with Over-the-Air (OTA) Incremental updates, full OS updates. Signing of packages and update images, server authentication and other key considerations for securely deploying updates.

Secure Manufacturing

Manufacturing Protection App Note

 

Manufacturing Protection Verification tool

 

Secure Manufacturing Training

Guidance to secure manufacturing in supported i.MX devices.

Reference verification tool provided to authorize products with this feature enabled.

Manufacturing Protection: Training on how to provision Sensitive Material in an Unsecure Environment

Public Key Cryptography using CAAM Secure Key

Strengthening Public Key Cryptography using CAAM Secure Key

Source Code

Leveraging the i.MX CAAM module to ensure the transfer of
confidential data upon insecure channels using ECDSA secure keys

Secure Storage

i.MX Encrypted Storage Using CAAM Secure Keys

Understanding SECO Secure Storage and Non-Volatile Memory Management 

This document provides steps to run storage encryption at the block
level using DM-Crypt taking advantage of the secure key feature.

This document describes some of the key concepts related to the Security Controller secure storage and non-volatile memory management. 

Securing Data

Demo Application to Generate Red/Black Blobs Using CAAM and Encrypt/Decrypt Data

Source Code

This document provides instructions and steps on how to set up and run a
demo application to generate both red and black key blobs and use them to encrypt and decrypt data.

Enhanced OpenSSL using OP-TEE

Enhanced OpenSSL on i.MX Processors 

Source Code

The purpose of this document is to describe how to add the support of
accelerated OP-TEE OS with CAAM on top of OpenSSL. 

On The Fly AES Decryption

OTFAD App Note

OTFAD Tool 

OTFAD support in i.MX 7ULP Application Processor

Tampering Application 

Tampering Application on i.MX 7D SabreSD Board

Source Code 

The document describes the steps required for software configuration and physical setup for both passive and active tampering on i.MX 7D.

Android™ Security User's Guide & User's Guide


  

 
 

Guide for customization work on security features supported
by i.MX Android software. It provides an overview of the i.MX Android security features and it focuses on how to configure and use these security features.

 
 

 User Guide provides instructions for:
• Downloading, patching, and building the software components that create the Android™ image.
• Hardware/software configurations for programming the boot media and
Building OTA update packages.

i.MX Chip Lifecycle

Transitioning the Chip Lifecycle to Field Return OEM

This application note introduces the chip lifecycle concept. The document also describes how to move the chip lifecycle from the OEM Closed lifecycle to the Field Return OEM lifecycle with the SPSDK tool on EdgeLock Secure Enclave (Advanced Profile) (ELE-AP) based i.MX devices.

i.MX Fuse Usage

Fuse Usage on i.MX Devices 

This application note covers fuse usage and various restrictions covering both  EdgeLock Secure Enclave (Advanced Profile) (ELE-AP) based i.MX devices and non-ELE based devices.

i.MX ROMs Log Events

i.MX ROMs Log Events

This document describes the details of ROM log events for i.MX 6/7/8/9 series ROM. 

Device Recovery 

HABv4 closed device recovery using UUU

Certain i.MX devices require the DCD pointer in IVT to be cleared before singing the recovery image. This document describes this procedure.

EdgeLock 2GO 

EdgeLock 2GO Services for MPU and MCU

 

 

EdgeLock 2GO Provisioning via Cloud Flow for MPUs

This application note introduces various methods that the EdgeLock 2GO service can be used with MCU and MPU devices and the features available for each method.

This document offers an outline of the EdgeLock 2GO platform and discusses the “Device provisioning via cloud” flow to connect the ELE based NXP devices to the EdgeLock 2GO cloud server.

 

Secure Elements

Quick start guide for EdgeLock™ SE05x & i.MX 8M

Quick start guide for EdgeLock™ SE050 & i.MX 6UltraLite

Quick start guide for A71CH & i.MX 6UltraLite

Ease ISA/IEC 62443 compliance with EdgeLock SE05x 

 Interfacing Secure Elements with the i.MX 

Binding a host device to EdgeLock SE05x

Binding MCUs with TrustZone® and Cryptographic Acceleration and Assurance Module (CAAM) to SE050x Secure Element

Known Limitations & Guidelines

Known limitations and guidelines document

This page contains known limitations in various IPs with i.MX processors.

i.MX Security Community 

i.MX Security community page

This is the parent page for various collateral related to security on i.MX Application Processors including public vulnerabilities

Vulnerability Management

Vigiles™ Software | NXP

Vigiles is a Software Composition Analysis (SCA) tool that helps generate and analyze a Software Bill of Materials (SBOM) for publicly known cybersecurity vulnerabilities, particularly CVEs. Vigiles is optimized for embedded systems, and it provides a complete vulnerability lifecycle management tool.


 

 


 

 

Training: Best Practices for Triaging Common Vulnerabilities and Exposures (CVEs) in Embedded System...

Training: Introducing: Vigiles

Training: Full Life-Cycle Security Maintenance of Embedded Linux BSPs

Training: BSP Security Maintenance - Best Practices for Vulnerability Monitoring and Remediation

i.MX Security Applications

GitHub - i.MX Security Apps

 

GitHub for NXP

Contains security applications like:

- CAAM demo applications

- Enhanced OpenSSL using OP-TEE

- HSM SHE examples

- Demo CAAM Blobs

- Manufacturing protection verification tool

Security Reference Manuals

Link to Various i.MX Security Reference Manuals 

 

 

Linux BSP Reference Manual

Linux BSP and Reference Manuals

 

PQC

Post-Quantum Cryptography 

 

Post-Quantum Secure TLS 1.3 on Application MPUs | NXP Semiconductors

 

Landing page with numerous Post-Quantum Cryptography resources and links to devices which support PQC

 

This session delves into how post-quantum cryptography, hardware security modules (HSMs) and trusted platforms through the EdgeLock® Secure Enclave.

Security Certification

PSA Level 1: NXP PSA L1 Certified Products

PSA Level 2: EdgeLock Secure Enclave 

PSA Level 3: i.MX 93 EdgeLock Secure Enclave

SESIP 1: i.MX 7ULP

SESIP 2: EdgeLock Secure Enclave

CAVP

i.MX 8ULP AES

i.MX 8ULP DRBG

Please contact your NXP representative on the latest processor security certification status 

CRA  & Security Compliance

EU Cyber Resilience Act (CRA) 

 

 

 

Ease CRA Compliance with i.MX 93 

 

 

Ease ISA/IEC 62443-4-2 Compliance with i.MX 8ULP

Ease ISA/IEC 62443-4-2 Compliance with i.MX 8XLite

NXP is actively preparing for CRA implementation. This Web page gives an overview as part of this effort, NXP will provide clear statements outlining how our product families will comply with the applicable CRA classes.

This document addresses OEMs who want to understand how i.MX 93 can facilitate the implementation of CRA requirements

 

Describes how i.MX SoCs can be used to facilitate the implementation of ISA/IEC 62443-4-2 requirements.

 

 

Security Blogs

Securing Tomorrow: NXP’s Post-Quantum Cryptography Strategy

 

U.S. Cyber Trust Mark: NXP Is Ready for the Paradigm Shift with EdgeLock® Assurance Program

Securing Your Industrial Systems with IEC 62443

 

IoT Security Just Got Easier: EdgeLock 2GO Programming Partners Simplify Device Provisioning 

This article explores how NXP’s portfolio enables seamless PQC adoption across new and existing products

U.S. Cyber Trust Mark: Security Guidance for IoT Product Developers

 

How NXP Supports Customers to Achieve 62443 Compliance

EdgeLock 2GO service gives device OEMs a secure, simple and flexible way to provision and manage device credentials, over the entire lifecycle of the device.

Security Whitepapers

Security Primitives: Requirements in (I)IoT Systems 

SECURING-INDUSTRIAL-IOT 

Security Subsystems for System-on-Chip (SoC) Solutions  

Functional Safety and Security: Essential and Complementary Disciplines for Modern Systems 

The Emergence of Post-Quantum Cryptography 

Post-Quantum Cryptography 

A solution for 360 degree Industrial Internet Security/ABB-MSFT-NXP 

 

 

100%が役に立ったと言っています (4/4)
バージョン履歴
最終更新日:
‎07-02-2026 06:18 PM
更新者: