RT1050 - setting up FTP Server

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

RT1050 - setting up FTP Server

1,443 次查看
shai_b
Senior Contributor II

Hi team,

My customer is trying to implement an FTP server into our RT1050 chipset.

they need to set up an FTP server since they are working with an IP camera that captures pictures when there is a movement and then saving it sending the pic via an FTP server.

so they are planning to implement FTP server into our RT1050 to hosting the camera and store the picture for later processing.

Could you please guide us on how to implement such a FTP server.

looking forward to your kind response.

Thanks in advance 

kind regards,

Shai 

标签 (1)
标记 (2)
0 项奖励
回复
1 回复

1,378 次查看
mjbcswitzerland
Specialist V

Hi

See https://www.utasker.com/iMX/RT1050.html

which has an integrated solution with FTP server which allows retrieving file saved on the RT 1050 in HyperFlash or SD card (if configured further it can also do it from a USB memory stick).
Alternatively it can be configured as FTP client to automatically push such files to a remote FTP server.

FTP server: https://www.utasker.com/docs/uTasker/uTaskerFTP.PDF
FTP client: https://www.utasker.com/docs/uTasker/uTaskerFTP_client.pdf

Regards

Mark
[uTasker project developer for Kinetis and i.MX RT]

0 项奖励
回复