SDRAM Bootable Image

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SDRAM Bootable Image

1,476 Views
james_moore
Contributor I

Is there an example/ guide available for an SDRAM bootable image on the RT1052?

I have tried to convert one of the SDK sample project into SDRAM bootable image but unable to boot from flash

 

SDK example projects (which has ethernet-wifi, LWIP, AWS, and Iot module)

  1. “evkbimxrt1050_Aws_aws_shadow_wiced
  2.  evkbimxrt1050_AWS_aws_greengrass_discovery_enet"

 

I have noticed, if  project is based on the “ethernet / wifi” or LWIP”  the SDRAM boot issue arise (irrespective of Flash memory ).

Thanks

Labels (1)
0 Kudos
Reply
1 Reply

1,406 Views
Sabina_Bruce
NXP Employee
NXP Employee

Hello James,

Hope you are doing well.

I recommend to begin with the following document:

https://community.nxp.com/docs/DOC-340655 

It provides the steps necessary to create the bootable image for sdram.

Best Regards,

Sabina

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

----------------------------------------------------------------------------------------------------------------------- 

0 Kudos
Reply