Hi,
I've used the sample code of CCC command to send the large bytes address, the code I wrote as below:
int main(void)
{
//Skip the I3C master config parts.
i3c_callArm();
}
void i3c_callArm(void)
{
display_ccc_status(i3c_callAr());
return;
}
enum I3C_COMM_STATUS i3c_callAr(void)
{
uint8_t Arm_DA_Reg_00 = 0x40;
uint8_t Arm_DA_Reg_01 = 0x13;
uint8_t Arm_DA_Reg_02 = 0x06;
uint8_t Arm_DA_Reg_03 = 0x00;
uint8_t aux_ccc_param[CCC_FRAME_PARAM_ARRAY_SIZE];
i3c_ccc_fsm_param_reset(aux_ccc_param);
aux_ccc_param[CCC_FRAME_NOF_SEGMENTS ] = 1;
aux_ccc_param[CCC_FRAME_SEG1_ADDR ] = Arm_DA; //Dynamic Address of slave is 0x55
aux_ccc_param[CCC_FRAME_SEG1_WRD ] = CCC_ADDR_WR;
aux_ccc_param[CCC_FRAME_SEG1_DATA_FIRST] = CCC_FRAME_SEGx_DATA;
aux_ccc_param[CCC_FRAME_SEG1_DATA_CNT ] = 4;
aux_ccc_param[aux_ccc_param[CCC_FRAME_SEG1_DATA_FIRST] + 0] = Arm_DA_Reg_00;
aux_ccc_param[aux_ccc_param[CCC_FRAME_SEG1_DATA_FIRST] + 1] = Arm_DA_Reg_01;
aux_ccc_param[aux_ccc_param[CCC_FRAME_SEG1_DATA_FIRST] + 2] = Arm_DA_Reg_02;
aux_ccc_param[aux_ccc_param[CCC_FRAME_SEG1_DATA_FIRST] + 3] = Arm_DA_Reg_03;
// Second segment: read 8 bytes from Arm DA
aux_ccc_param[CCC_FRAME_SEG2_ADDR ] = Arm_DA; //Dynamic Address of slave is 0x55
aux_ccc_param[CCC_FRAME_SEG2_WRD ] = CCC_ADDR_RD;
aux_ccc_param[CCC_FRAME_SEG2_DATA_FIRST ] = CCC_FRAME_SEGx_DATA + aux_ccc_param[CCC_FRAME_SEG1_DATA_CNT];
aux_ccc_param[CCC_FRAME_SEG2_DATA_CNT ] = 8;
return i3c_ccc_fsm(aux_ccc_param);
}
// specify parameters needed for CCC frames to be transmitted
enum CCC_PARAM
{
CCC_FRAME_NOF_SEGMENTS = 0,
CCC_FRAME_SEG1_ADDR, CCC_FRAME_SEG1_WRD, CCC_FRAME_SEG1_DATA_CNT, CCC_FRAME_SEG1_DATA_FIRST,
CCC_FRAME_SEG2_ADDR, CCC_FRAME_SEG2_WRD, CCC_FRAME_SEG2_DATA_CNT, CCC_FRAME_SEG2_DATA_FIRST,
CCC_FRAME_SEGx_DATA,
CCC_FRAME_PARAM_COUNT // DO NOT REMOVE THIS LINE!!!
};
According to above code, I expect that I can access the 0x40130600 and read 8 bytes data back.
However, the waveform shows that master only send 0x401306, then slave return a NACK then command stopped.
May I know what's the possible problem about this issue?
If you need more information to know this issue, please feel free to ask, thanks!