Hi
The HSUSB host has automatic reset timing that the users doesn't look to have any control over:

Normally hosts assert the reset for 10ms but I measure 55ms when the HSUSB asserts it.
A) A FS device reference connected to a PC

B: The same FS device connected to the i.MX RT that issues the reset command on detection
PORTSC1 |= (USBHS_PORTSC1_PR);

This is not an issue with the device being reset but is this quite large deviation from the standard 10ms time intentional?
Regards
Mark