Failed to execute MI command: StubSWODataSource: -interpreter - exec console "mon SWO datasource"

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Failed to execute MI command: StubSWODataSource: -interpreter - exec console "mon SWO datasource"

1,707 Views
oswaldo-153
Contributor III
 

 Hello, I am working with the imxrt1050 board, in mcuxpresso. I am developing a project with lvgl, when I debug the project it sends me the following error and my program does not run.

0 Kudos
Reply
1 Reply

1,694 Views
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
To provide the fastest possible support, I'd highly recommend you to implement the steps that are demonstrated in Get Started with the MIMXRT1050-EVK to confirm your board is good.
Next, I was wondering if you can introduce the process of creating your LVGL demo project.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply