Can I run OASIS on RT1060EVK

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can I run OASIS on RT1060EVK

Jump to solution
1,766 Views
akkdong
Contributor I

I have RT1060EVK but does not have SLN-VIZNAS-IOT. So I want to run sln_viznas_iot_elock_oobe example on RT1060EVK. 

I changed EVK to use HyperFlash & changed  sln_viznas_iot_elock_oobe project to run on EVK (memory setting, flash, ...) but it didn't run on it.

I also create a new project using OASIS library. but it didn't work.

Can I run OASIS on RT1060EVK? 

 

 

0 Kudos
Reply
1 Solution
1,756 Views
jeremyzhou
NXP Employee
NXP Employee

Thanks for your reply.
1. We do not need security features. so We want to change to a bootloader with no security features. Does it matter?
-- No.
2. We want to change device memory map. more & single application block. and more file system space. Does it matter?
-- No.
3. Does increasing the memory(Flash & SDRAM) increase the Max # of faces.
-- If need more persons to be supported in the future, this mostly relies on MCU computation power not flash/RAM size since the minimum size is very well optimized.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
3 Replies
1,759 Views
akkdong
Contributor I

Thank you for the fast reply.

I have a few more questions about sln_viznas_iot_elock_oobe  example on SLN-VIZNAS-IOT(RT106F)

 

1. We do not need security features. so We want to change to a bootloader with no security features. Does it matter?

2. We want to change device memory map. more & single application block. and  more  file system space. Does it matter?

3. Does increasing the memory(Flash & SDRAM) increase the Max # of faces.

 

Thanks advance.

0 Kudos
Reply
1,757 Views
jeremyzhou
NXP Employee
NXP Employee

Thanks for your reply.
1. We do not need security features. so We want to change to a bootloader with no security features. Does it matter?
-- No.
2. We want to change device memory map. more & single application block. and more file system space. Does it matter?
-- No.
3. Does increasing the memory(Flash & SDRAM) increase the Max # of faces.
-- If need more persons to be supported in the future, this mostly relies on MCU computation power not flash/RAM size since the minimum size is very well optimized.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply
1,761 Views
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
1) Can I run OASIS on RT1060EVK?
-- No, I'm afraid it's impossible t run the OASIS on i.MX RT1060 instead of i.MX RT106F.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply