variable mapping

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
3,372件の閲覧回数
leroynash
Contributor I
I ran out of space in SRAM_DTC and need to map some arrays to SRAM_OC (RAM3) the line: __DATA(RAM3) double g_F_k[NSTATE][NSTATE] = {{0.0}}; results in: ../source/filter/src/tight_coupling.c:30:1: warning: return type defaults to 'int' [-Wimplicit-int] 30 | __DATA(RAM3) double g_F_k[NSTATE][NSTATE] = {{0.0}}; // State Transition Matrix | ^~~~~~ ../source/filter/src/tight_coupling.c: In function '__DATA': ../source/filter/src/tight_coupling.c:30:1: error: parameter 'g_F_k' is initialized ../source/filter/src/tight_coupling.c:30:1: warning: braces around scalar initializer ../source/filter/src/tight_coupling.c:30:1: note: (near initialization for 'g_F_k') any ideas? Thanks Leroy
0 件の賞賛
返信
1 解決策
3,358件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Him
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
To place data item into a specific memory region, it should add the below code in the code project prior to using the __DATA macro.

#include <cr_section_macros.h>


TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
3,359件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Him
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
To place data item into a specific memory region, it should add the below code in the code project prior to using the __DATA macro.

#include <cr_section_macros.h>


TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信
3,343件の閲覧回数
leroynash
Contributor I

That simple, thanks

0 件の賞賛
返信
3,360件の閲覧回数
crist_xu
NXP Employee
NXP Employee

Try to use __attribute__() instead? 

0 件の賞賛
返信