usb problem

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

usb problem

2,318 次查看
eao
Contributor I

Hello, I have a confusion. Now I want to connect two identical development boards through USB for data interaction. I checked the example of USB, but I didn't see any example of communication between MCUs. Which one can I refer to? Modified example. The development board is RT1170, Thank you. 

0 项奖励
回复
3 回复数

2,312 次查看
jingpan
NXP TechSupport
NXP TechSupport

Hi @eao ,

Do you mean you want to connect two RT1170 board with USB? That is one board act as a master, the other act as a slave. You can download usb_device_cdc_vcom project to one board and usb_host_cdc to the other. These two project can be found in RT1170 SDK.

 

Regards,

Jing

0 项奖励
回复

2,304 次查看
eao
Contributor I

Thanks for the reply, it is probably this one, one as the master and one as the slave. I read the examples in the SDK and found that there is a difference between dev_cdc_vcom and dev_cdc_vcom_lite? thanks

0 项奖励
回复

2,299 次查看
jingpan
NXP TechSupport
NXP TechSupport

Hi @eao ,

All most same.

 

Regards,

Jing

0 项奖励
回复