usb problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

usb problem

2,317 Views
eao
Contributor I

Hello, I have a confusion. Now I want to connect two identical development boards through USB for data interaction. I checked the example of USB, but I didn't see any example of communication between MCUs. Which one can I refer to? Modified example. The development board is RT1170, Thank you. 

0 Kudos
Reply
3 Replies

2,311 Views
jingpan
NXP TechSupport
NXP TechSupport

Hi @eao ,

Do you mean you want to connect two RT1170 board with USB? That is one board act as a master, the other act as a slave. You can download usb_device_cdc_vcom project to one board and usb_host_cdc to the other. These two project can be found in RT1170 SDK.

 

Regards,

Jing

0 Kudos
Reply

2,303 Views
eao
Contributor I

Thanks for the reply, it is probably this one, one as the master and one as the slave. I read the examples in the SDK and found that there is a difference between dev_cdc_vcom and dev_cdc_vcom_lite? thanks

0 Kudos
Reply

2,298 Views
jingpan
NXP TechSupport
NXP TechSupport

Hi @eao ,

All most same.

 

Regards,

Jing

0 Kudos
Reply