system core clock control

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

system core clock control

Jump to solution
2,358 Views
yf2
Contributor III

Dear support,

 

I am testing a computing library on RT1170-EVK and I noticed that my SystemCoreClock reads out 528Mhz, not close to 1Ghz as expected.

Is there any simple method to boost the system core clock speed on RT1170-EVK? plain C code fragements are welcomed.

 

Regards,

yf

 

 

Tags (1)
0 Kudos
Reply
1 Solution
2,332 Views
Omar_Anguiano
NXP TechSupport
NXP TechSupport

Config Tools allows you preview the generated code for that configuration. You can download the standalone version of the tool so you can integrate the configuration on the IDE you are using: MCUXpresso Config Tools|Software Development for NXP Microcontrollers (MCUs) | NXP Semiconductors
MCUXpresso Config Tools currently supports the following toolchains:
• IAR Embedded Workbench
• Keil MDK uVision
• Arm GCC

If you have more questions do not hesitate to ask me.
Best regards,
Omar

View solution in original post

0 Kudos
Reply
5 Replies
2,347 Views
Omar_Anguiano
NXP TechSupport
NXP TechSupport

Hello
Hope you are well.
You can use config tools from MCUXpresso to generate the code that enables running the core at 1Ghz.

Omar_Anguiano_0-1658968798555.png

 

It is important to mention that only consumer grade RT1170 is able to run at 1GHz.

If you have more questions do not hesitate to ask me.
Best regards,
Omar

0 Kudos
Reply
2,343 Views
yf2
Contributor III

@Omar_Anguiano 

 

Thanks a lot for your information.

Currently I am not using the IDE and the "fsl_clock.h" librariess yet. I will see how to use the config tool.

If you know some simple code fragments, please also teach.

 

Regards,

yf2

0 Kudos
Reply
2,333 Views
Omar_Anguiano
NXP TechSupport
NXP TechSupport

Config Tools allows you preview the generated code for that configuration. You can download the standalone version of the tool so you can integrate the configuration on the IDE you are using: MCUXpresso Config Tools|Software Development for NXP Microcontrollers (MCUs) | NXP Semiconductors
MCUXpresso Config Tools currently supports the following toolchains:
• IAR Embedded Workbench
• Keil MDK uVision
• Arm GCC

If you have more questions do not hesitate to ask me.
Best regards,
Omar

0 Kudos
Reply
2,329 Views
yf2
Contributor III

@Omar_Anguiano 

Can I assume that the MCUXpresso Config Tools is not specific for EVK boards but also apply to customer boards?

Regards,

yf2

0 Kudos
Reply
2,321 Views
Omar_Anguiano
NXP TechSupport
NXP TechSupport

You´re correct, since the tool focus on the MCU.

Best regards,
Omar

0 Kudos
Reply