"Function called without core lock" when re-initializing LWIP with changed IP info

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

"Function called without core lock" when re-initializing LWIP with changed IP info

819 次查看
JamesNgo
Contributor III

I'm using RT1021 lwip stack and need to account for the IP info could be changed dynamically. This info is needed when initialize LWIP stack, below:

 

netifapi_netif_add(&g_netif, &netif_ipaddr, &netif_netmask, &netif_gw, &enet_config, EXAMPLE_NETIF_INIT_FN,tcpip_input);


netifapi_netif_set_default(&g_netif);


netifapi_netif_set_up(&g_netif);

My questions are:

1. Is there such API de_init_lwip to properly delete/remove previously lwip stack setup with old IP info to repeat the re-initialization with new IP info? (I tried to re-init anyways this without the non existing de_init API and ran into a ASSERT code halt "Function called without core lock").

2. How do I handle properly when getting the new IP info to re-initialize lwip stack to effect the new IP?

 

thanks.

 

 

 

标签 (1)
0 项奖励
回复
1 回复

785 次查看
Gavin_Jia
NXP TechSupport
NXP TechSupport

Hi @JamesNgo ,

Thanks for your interest in NXP MIMXRT series!

LWIP is an open source lightweight networking stack, it does not provide an API such as lwip_deinit(). including the SDK provided by NXP does not change this.There are some APIs in LWIP that are thread-unsafe, and the error you are experiencing should be for this reason.

Consider using the netif_remove() function to remove the network interface, removing the current network interface configuration.And use mem_free() to manually free the memory resources associated with the network interface.Ensure that all related tasks and data transfers are stopped before removing the interface to avoid resource conflicts.

Best regards,
Gavin

0 项奖励
回复