mp3 decoder optimized for M7 core

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

mp3 decoder optimized for M7 core

2,749 Views
cerma
Contributor IV

Hi All,

I need to make mp3 player on imxRT1060. It will read from the SD card and send the decoded data to the I2S codec. Does NXP have any library for SW mp3 decoder optimized for M7 (imxRT). Is there a example mp3 decoder project for imxRT(MCUXpresso)? Or, Do I have to use Helix decoder or any one else. Is anybody able to help me?

Thank you.

J. C.

Tags (3)
0 Kudos
Reply
1 Reply

2,630 Views
jingpan
NXP TechSupport
NXP TechSupport

Hi Jaroslav,

The MP3 codec components are not implemented in our the demo software  due to a source code license conflict between the NXP software and the available open MP3 sources.  Below is link of LPC app note, which also may be helpful for customers, using i.MX RT1050.
 https://www.nxp.com/docs/en/application-note/LPC4357-Internet-Radio-MP3-Player-Demo.pdf 

https://www.nxp.com/docs/en/application-note/AN11178.zip 

Regards,

Jing

0 Kudos
Reply