Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
1) Can I safely use SPDIF_TransferSendEDMA within the eDMA callback interrupt?
Or is there a more basic way to trigger the same sized transfer over and over within the callback?
-- In my opinion, I'd highly recommend you to use the scatter-gather feature to configure the DMA to prepare the next transfer automatically, then you can activate the DMA easily in the callback function when completing the previous DMA transfer.
Have a great day,
TIC
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------