imx Rt595 I3C interface

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx Rt595 I3C interface

ソリューションへジャンプ
2,328件の閲覧回数
gilmotta2
Contributor II

Hello All,

Can anyone please share or point an I3C sample code for the RT595 to me? I would like to run a test sending bytes over I3C. I'm using the MIMXRT595-EVK and I did not find any sample code for this EVK.

Thanks,

Gil

#RT595

0 件の賞賛
返信
1 解決策
2,317件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi @gilmotta2 ,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
To provide the fastest support, I'd like to refer to the I3C demo in the SDK for RT 595.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,298件の閲覧回数
Mahesh_Chandra
NXP Employee
NXP Employee

Hi,

SDK has two projects. One project is set up for I3C master and the other project is set up for I3C slave.

You can directly use these projects after connecting two MIMXRT595-EVK boards together as mentioned

in the code examples.

0 件の賞賛
返信
2,318件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi @gilmotta2 ,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
To provide the fastest support, I'd like to refer to the I3C demo in the SDK for RT 595.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the

0 件の賞賛
返信