Thank you for your interest on our RT1180!
I do not have an RT1180 to test with me, as I am not part of the NPI process of the RT1180, so I can not reproduce this issue on my bench. For this particular time, I advice to contact your dedicated NXP representative, to get more dedicated help.
I still checked your project, and I saw that you linked your application to the HyperRAM address space, I wonder if the issue you are reporting can be reproduced all the time. But I suggest you to check with the XMCD that the MCUxpresso Secure Provisioning embeds when programming your image. With the tool, you can generate a bootable image and program over LPUART1 or USB1. Below a reference picture.
I hope this helps you!
Diego
Thanks Diego, i will try but this is only a test. i must use hyper ram with debugger but i want to understand why all example for M7 present oin SDK works only with internal ram, isn't checked wirh flash or external ram? i understand that the mcu is not released in this date but, as me i need to check the mcu to decide if use nxp or another brand, and i have a lot of problem for simple things..
anyway if you have a chance to use an 1180 board and test it runtime shuld appreciate.
Simone

Thank you for your reply, I understand your feeling, agian we appreaciate your interest.
Let me check and discuss about this situation. I want to know which SDK release and toolchain you are using, could you let know that?
Update: maybe this will help to explain the issue: see RAW/POR image switch from the new MCUXpresso https://mcuxpresso.nxp.com/mcuxsdk/latest/html/boards/evkmimxrt1180/gettingStarted/topics/bootable_i...
Diego