iMXRT1062 External Hardware Debugger

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

iMXRT1062 External Hardware Debugger

2,476件の閲覧回数
ahmed_mostafa
Contributor II

Hi,

I purchased this board from Sparkfun: Teensy 4.0 - DEV-15583 - SparkFun Electronics 

And I would like to program it using the MCUXpressoIDE. Do I need to purchase an additional debugger to be able to program this uC? If so, which debugger should I use and how does it connect?

Thanks,

Ahmed

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

2,364件の閲覧回数
danstipe
Contributor I

Hi Filipe,

Could you please post the Felipe, to Ahmed's question regarding the MCUXpresso IDE?

Is an additional debugger available for the i.MXRT1062? If so, how is it connected?

Kind Regards,

Dan

0 件の賞賛
返信

2,372件の閲覧回数
FelipeGarcia
NXP Employee
NXP Employee

Hi Ahmed,

 

I am glad to hear that you found the solution. Thanks for sharing this with the community!

 

Have a great day,

Felipe

0 件の賞賛
返信