iMXRT1021 blowing efuse via executable code?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

iMXRT1021 blowing efuse via executable code?

跳至解决方案
2,358 次查看
t_thurgood
Contributor III

Hi,

We are using the iMXRT1021 and need to blow efuses via executable code.

I have looked at IMXRT1020RM.pdf, but this describes efuse functionality, but not usability. At the moment we can blow efuses either using Blhost/flashloader or MCU Boot Utility/Flashloader.

Is there an application note explaining internal efuse programming?

Can anyone advise how to do this?

I have found a reference to EFUSE_PROG_SUPPLY_GATE which I assume needs to be set, then what?

br,

Tony

1 解答
2,274 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi Tony Thurgood,

Thank you for your interest in NXP Semiconductor products and
for the opportunity to serve you.
I'd like to suggest you refer to the ocotp demo which is from the SDK library, this demo demonstrates that uses the KSDK software to access eFuse map.

TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
4 回复数
2,274 次查看
carstengroen
Senior Contributor II

Tony,

perhaps this can be of some help: https://community.nxp.com/thread/492451 

(I assume the same procedure for the 102x ?!)

2,274 次查看
t_thurgood
Contributor III

Hi Carsten,

Thanks for the link.

I think that is all useful information to get this working for me.

br,

Tony

2,275 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi Tony Thurgood,

Thank you for your interest in NXP Semiconductor products and
for the opportunity to serve you.
I'd like to suggest you refer to the ocotp demo which is from the SDK library, this demo demonstrates that uses the KSDK software to access eFuse map.

TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复
2,274 次查看
t_thurgood
Contributor III

Hi Jeremy,

Thanks for the info.

best regards,

Tony

0 项奖励
回复