iMXRT1010 SWD interface disabled

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

iMXRT1010 SWD interface disabled

1,615件の閲覧回数
ladislav_piroha
Contributor I

We built a new hardware based on iMXRT1011 and spent several hours with SWD interface bring up. MCU refused re-programming requests over SWD interface. Then we found 10K pull_down resistor on JTAG_MOD (GPIO_AD_11) in RT1010 reference board schematics that enables SWD interface. Funny thing is that I could not find anything mentioned IMXRT1010RM datasheet.
Fuse DAP_SJC_SWD_SEL  is set to 0 so I would expect that SWD is enabled by default, but it's somehow overridden by GPIO_AD_11 and JTAG is selected when GPIO_AD_11 is floating.

0 件の賞賛
返信
1 返信

1,599件の閲覧回数
victorjimenez
NXP TechSupport
NXP TechSupport

Hello, 

Thanks for your feedback, I will pass it to the documentation team. 

Also, when creating your own board besides using as reference the reference manual and the datasheet, I highly recommend you to use also the Hardware Development Guide for the RT1010. 

https://www.nxp.com/docs/en/user-guide/MIMXRT1010HDUG.pdf

 

Have a great day,

Victor

-------------------------------------------------------------------------------

Note:

- If this post answers your question, please click the "Mark Correct"button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored

Please open a new thread and refer to the closed one, if you have a related question at a later point in time.

-------------------------------------------------------------------------------

 

0 件の賞賛
返信