We built a new hardware based on iMXRT1011 and spent several hours with SWD interface bring up. MCU refused re-programming requests over SWD interface. Then we found 10K pull_down resistor on JTAG_MOD (GPIO_AD_11) in RT1010 reference board schematics that enables SWD interface. Funny thing is that I could not find anything mentioned IMXRT1010RM datasheet.
Fuse DAP_SJC_SWD_SEL is set to 0 so I would expect that SWD is enabled by default, but it's somehow overridden by GPIO_AD_11 and JTAG is selected when GPIO_AD_11 is floating.
Hello,
Thanks for your feedback, I will pass it to the documentation team.
Also, when creating your own board besides using as reference the reference manual and the datasheet, I highly recommend you to use also the Hardware Development Guide for the RT1010.
https://www.nxp.com/docs/en/user-guide/MIMXRT1010HDUG.pdf
Have a great day,
Victor
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct"button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------