Hi everyone,
I would like to control an ADC chip via FlexIO SPI.
How can I influence the clock cycle between the slave select
negating and before the next transfer?
In SDK examples this time is always an SPI clock.
I need longer time for CS high before the next transfer started.
Is that possible?
Hi Johann,
Sorry for the later reply.
I did a test with MIMXRT1060-EVK board with [flexio3_spi_int_lpspi_transfer_master] demo.
I could find your mentioned behavior.
I want to modify the Flexio spi driver at <fsl_flexio_spi.c> file FLEXIO_SPI_MasterInit() function without success.
So far, when customer write data to shifter buffer, the FlexIO_SPI engine will start to transfer data.
So, customer can set TRANSFER_SIZE to 1, which means only transfer one byte, and then call FLEXIO_SPI_MasterTransferNonBlocking function again to transfer another byte with related time interval.
#define TRANSFER_SIZE 1U /*! Transfer dataSize */
/*Start master transfer*/
masterXfer.txData = masterTxData;
masterXfer.rxData = masterRxData;
masterXfer.dataSize = TRANSFER_SIZE;
masterXfer.flags = kFLEXIO_SPI_8bitMsb;
isMasterTransferCompleted = false;
FLEXIO_SPI_MasterTransferNonBlocking(&spiDev, &g_m_handle, &masterXfer);
for(int i = 0; i<0xfff; i++)
{
asm("nop");
}
while (!(isMasterTransferCompleted))
{
}
isMasterTransferCompleted = false;
FLEXIO_SPI_MasterTransferNonBlocking(&spiDev, &g_m_handle, &masterXfer);
for(int i = 0; i<0xffff; i++)
{
asm("nop");
}
while (!(isMasterTransferCompleted))
{
}
isMasterTransferCompleted = false;
FLEXIO_SPI_MasterTransferNonBlocking(&spiDev, &g_m_handle, &masterXfer);
for(int i = 0; i<0xfff; i++)
{
asm("nop");
}
while (!(isMasterTransferCompleted))
{
}
isMasterTransferCompleted = false;
FLEXIO_SPI_MasterTransferNonBlocking(&spiDev, &g_m_handle, &masterXfer);
The test result is below:
I couldn't change the Flexio_spi low level driver, just called related API using a tricky way.
Thanks for the attention.
best regards,
Mike
Hi Mike,
thanks for the answer.
The idea is to control 4x the AD7699 with the FlexIO.
SPI-Enable, SPI-Clock and SPI-MOSI connected parallel to all ADC's,
just read in the MISO from each AD7699 via FlexIO extra.
Would that be possible in principle with FlexIO?
Can you give me a hint how to expand the existing driver?
best regards
Johann
Hi Johann,
First of all, sorry for the later reply.
It is possible to use FlexIO with more MISO pins.
Please refer current <fsl_flexio_spi.c> file FLEXIO_SPI_MasterInit() function to add three more shifter for rx.
And it also need to set required pins with FlexIO function.
Wish it helps.
best regards,
Mike
Hi Mike,
I have implemented 2x AD7699 read in parallel SPI.
It works so far.
Only I was surprised that the SDK MIMXRT1064.h SHIFTBUFBIS [4] is limited to 4. In the i.MX RT1064 rtreference manual page 2925 the registers are described with SHIFTBUFBIS0 -
SHIFTBUFBIS7.
Is it a survival of the i.MXRT1060 or what's right there?
best regards
Johann
Hi Johann,
Sorry for the later reply.
I did a test with MIMXRT1064-EVK board, the debug info showed there with 4 shifter with one FlixIO module.
The RT1064 reference manual with incorrect info.
I will report that document issue.
Thanks and have a nice day!
best regards,
Mike