i.MXRT1176 USDHC2 and FlexSPI(Octal Flash) pin conflict

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MXRT1176 USDHC2 and FlexSPI(Octal Flash) pin conflict

ソリューションへジャンプ
729件の閲覧回数
许贻辉2023
Contributor I

i.MXRT1176 USDHC2 and FlexSPI(Octal Flash) pin conflict, I checked IMXRT1170RM, if I want to use FlexSPI1 to start from Octal Flash, then pin conflict with USDHC2 (8-wire mode), Any recommended solutions for tech support?

FlexSPI1-A-B.png

FlexSPI1.png

USDHC.png
In addition, FlesSPI1 and FlexSPI2; Is there any performance difference between connecting Octal Flash? Such as clock frequency, prefetching capabilities.

0 件の賞賛
返信
1 解決策
712件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @许贻辉2023 ,

   Good question!

   If just in FlexSPI1 and the USDHC2 (8-wire mode), no way, must one interface is not used.

   But, RT1170 is powerful, it have two FlexSPI, you totally can boot from the FlexSPI2, that won't conflict with the USDHC2 (8-wire mode).

   More details, please read this blog:

https://www.cnblogs.com/henjay724/p/15139381.html

  FlesSPI1 and FlexSPI2 connect to the octal flash, is the same performance, just the map address is different.

 

Wish it helps you!

Best Regards,

Kerry

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
713件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @许贻辉2023 ,

   Good question!

   If just in FlexSPI1 and the USDHC2 (8-wire mode), no way, must one interface is not used.

   But, RT1170 is powerful, it have two FlexSPI, you totally can boot from the FlexSPI2, that won't conflict with the USDHC2 (8-wire mode).

   More details, please read this blog:

https://www.cnblogs.com/henjay724/p/15139381.html

  FlesSPI1 and FlexSPI2 connect to the octal flash, is the same performance, just the map address is different.

 

Wish it helps you!

Best Regards,

Kerry

0 件の賞賛
返信