i.MXRT1176 USDHC2 and FlexSPI(Octal Flash) pin conflict

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MXRT1176 USDHC2 and FlexSPI(Octal Flash) pin conflict

Jump to solution
728 Views
许贻辉2023
Contributor I

i.MXRT1176 USDHC2 and FlexSPI(Octal Flash) pin conflict, I checked IMXRT1170RM, if I want to use FlexSPI1 to start from Octal Flash, then pin conflict with USDHC2 (8-wire mode), Any recommended solutions for tech support?

FlexSPI1-A-B.png

FlexSPI1.png

USDHC.png
In addition, FlesSPI1 and FlexSPI2; Is there any performance difference between connecting Octal Flash? Such as clock frequency, prefetching capabilities.

0 Kudos
Reply
1 Solution
711 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @许贻辉2023 ,

   Good question!

   If just in FlexSPI1 and the USDHC2 (8-wire mode), no way, must one interface is not used.

   But, RT1170 is powerful, it have two FlexSPI, you totally can boot from the FlexSPI2, that won't conflict with the USDHC2 (8-wire mode).

   More details, please read this blog:

https://www.cnblogs.com/henjay724/p/15139381.html

  FlesSPI1 and FlexSPI2 connect to the octal flash, is the same performance, just the map address is different.

 

Wish it helps you!

Best Regards,

Kerry

View solution in original post

0 Kudos
Reply
1 Reply
712 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @许贻辉2023 ,

   Good question!

   If just in FlexSPI1 and the USDHC2 (8-wire mode), no way, must one interface is not used.

   But, RT1170 is powerful, it have two FlexSPI, you totally can boot from the FlexSPI2, that won't conflict with the USDHC2 (8-wire mode).

   More details, please read this blog:

https://www.cnblogs.com/henjay724/p/15139381.html

  FlesSPI1 and FlexSPI2 connect to the octal flash, is the same performance, just the map address is different.

 

Wish it helps you!

Best Regards,

Kerry

0 Kudos
Reply