i.MXRT1170: XBAR problems with chained DMAs

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MXRT1170: XBAR problems with chained DMAs

Jump to solution
1,961 Views
michael_fischer
Contributor III

Hello forum,
Hello @Kan_Li 

last time I got the hint from you that the “XBARA1_InputDmaDone0” is only an pulse and not a high signal. Reference is made to my old post here: https://community.nxp.com/t5/i-MX-RT/i-MXRT1170-How-to-route-kXBARA1-InputDmaDone0-through-XBAR1/m-p... 

Reference is made to the i.MXRT1170-EVKB board.

The “DmaDone” with the XBAR is working if the DMA is started by the write to the SERQ register. In this case the setup of the DMA, here DMA1 looks like:

static void DMAInitChannel1 (void)
{
   edma_transfer_config_t transferConfig;

   DMAMUX_EnableAlwaysOn(DMAMUX0, 1, true);
   DMAMUX_EnableChannel(DMAMUX0, 1);

   EDMA_CreateHandle(&dmaHandle1, DMA0, 1);
   EDMA_ResetChannel(dmaHandle1.base, dmaHandle1.channel);

   memset(&transferConfig, 0x00, sizeof(transferConfig));
   EDMA_PrepareTransfer(&transferConfig,
                        (void*)&srcBuffer1[0],
                        32,
                        (void*)&destBuffer[8],
                        32,
                        32,
                        32,
                        kEDMA_MemoryToMemory);
   EDMA_SubmitTransfer(&dmaHandle1, &transferConfig);
   EDMA_SetMajorOffsetConfig(DMA0, 1, -32, -32);
   EDMA_SetCallback(&dmaHandle1, EDMA_Callback, NULL);
   XBARA_SetSignalsConnection(XBARA1, kXBARA1_InputDmaDone1,  kXBARA1_OutputIomuxXbarInout38);

} /* DMAInitChannel1 */

Here the DMA1 can be started several times with the following command:

EDMA_StartTransfer(&dmaHandle1);

Every time the DMA1 is working, and the GPIO pulse is available on the oscilloscope.

========================================================================

But if I used a chained DMA, that mean I will linked DMA0 with DMA1 and start DMA0. The pulse is not available anymore on the oscilloscope. The new code looks like:

static void DMAInitChannel0 (void)
{
   edma_transfer_config_t transferConfig;

   DMAMUX_EnableAlwaysOn(DMAMUX0, 0, true);
   DMAMUX_EnableChannel(DMAMUX0, 0);

   EDMA_CreateHandle(&dmaHandle0, DMA0, 0);
   EDMA_ResetChannel(dmaHandle0.base, dmaHandle0.channel);

   memset(&transferConfig, 0x00, sizeof(transferConfig));
   EDMA_PrepareTransfer(&transferConfig,
                        (void*)&srcBuffer0[0],
                        32,
                        (void*)&destBuffer[0],
                        32,
                        32,
                        32,
                        kEDMA_MemoryToMemory);
   EDMA_SubmitTransfer(&dmaHandle0, &transferConfig);
   EDMA_SetMajorOffsetConfig(DMA0, 0, -32, -32);

} /* DMAInitChannel0 */

static void DMAInitChannel1 (void)
{
   edma_transfer_config_t transferConfig;

//   DMAMUX_EnableAlwaysOn(DMAMUX0, 1, true);
//   DMAMUX_EnableChannel(DMAMUX0, 1);

   EDMA_CreateHandle(&dmaHandle1, DMA0, 1);
   EDMA_ResetChannel(dmaHandle1.base, dmaHandle1.channel);

   memset(&transferConfig, 0x00, sizeof(transferConfig));
   EDMA_PrepareTransfer(&transferConfig,
                        (void*)&srcBuffer1[0],
                        32,
                        (void*)&destBuffer[8],
                        32,
                        32,
                        32,
                        kEDMA_MemoryToMemory);
   EDMA_SubmitTransfer(&dmaHandle1, &transferConfig);
   EDMA_SetMajorOffsetConfig(DMA0, 1, -32, -32);
   EDMA_SetCallback(&dmaHandle1, EDMA_Callback, NULL);
   XBARA_SetSignalsConnection(XBARA1, kXBARA1_InputDmaDone1,  kXBARA1_OutputIomuxXbarInout38);

   EDMA_SetChannelLink(DMA0, 0, kEDMA_MajorLink, 1);

} /* DMAInitChannel1 */

And the chained  DMA can be started with:

EDMA_StartTransfer(&dmaHandle0);

Here the data will be transferred by DMA0 and DMA1, but the “DmaDone1” will not produce the GPIO pulse anymore.

It looks that the XBAR functionality is only working here if the DMA was started by the SERQ regsiter and not internaly by the link functionality.

Do you have any hints for me?

Best regards,
Michael

 

0 Kudos
Reply
1 Solution
1,584 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @michael_fischer ,

 

It has been confirmed by the design team, it is IP behavior. If triggered by START bit from SW or Channel Link, there is no minor loop done signal generated.

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

View solution in original post

9 Replies
1,930 Views
michael_fischer
Contributor III

Some more information.

It looks that the XBAR functionality is only working here if:

  • the DMAMUX0.CHCFG[x].ENBL bit is set for the corresponding DMA channel and,
  • the DMAMUX0.CHCFG[x].A_ON bit is set for the corresponding DMA channel and,
  • the DMA was started by the SERQ register.

It looks that it is not working if it is started:

  • internally by the link functionality, or
  • by setting the TCDx_CSR.START bit of the corresponding DMA channel
0 Kudos
Reply
1,854 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @michael_fischer ,

 

I believe that is due to DMA channel 1 is a linked channel, as I can always catch the done signal out of DMA channel 0, even it was linked to channel 1. I will check with the expert if it is an expected result.

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply
1,794 Views
michael_fischer
Contributor III

Hello @Kan_Li ,

Is there an update from the experts yet?

Best regards,
Michael

 

0 Kudos
Reply
1,585 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @michael_fischer ,

 

It has been confirmed by the design team, it is IP behavior. If triggered by START bit from SW or Channel Link, there is no minor loop done signal generated.

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

1,575 Views
michael_fischer
Contributor III

Hello @Kan_Li ,

>there is no minor loop done signal generated.
I think there is no major loop done signal too.

Best regards,
Michael

0 Kudos
Reply
1,568 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @michael_fischer ,

 

Yes, you are right!

 

Best Regards,

Kan

0 Kudos
Reply
1,776 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @michael_fischer ,

 

This issue has been submitted to Designer for investigation, and I will let you know when I have any more info from there.

 

Thanks for your patience!

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply
1,673 Views
michael_fischer
Contributor III

Hello @Kan_Li ,

Is there an update from the Designer yet?

Best regards,
Michael

0 Kudos
Reply
1,662 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @michael_fischer ,

 

This issue has been reproduced here but the designer is still investigating the root cause, and the expert also recommended reducing the EDMA clock to resolve the low pulse peak issue, but reducing the EMDA clock may lower the performance, you may balance it according to the application requirements.

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply