Hi guys,
I have been finding out how the different LCDIF_Dx signals are mapped to RGB data.
In the case of the IMXRT1602 EVK, the designer used the RGB565 color space. I would like to know how to map the LCDIF_Dx signals to other color spaces.
I would appreciate if someone at NXP can check the following table I made to see if I got the idea.
Thank you!
Patricio
===============================
RGB332 - 8 BIT COLOR(3R,3G,2B) ORGANIZED AS 8 BIT (BYTE)
RRGG.GBBB
D00 - B0
D01 - B1
D02 - B2
D03 - G0
D04 - G1
D05 - G2
D06 - B0
D07 - B1
RGB555 - 15 BIT COLOR(5R,5G,5B) ORGANIZED AS 16 BIT (HALF WORD)
xRRR.RRGG.GGGB.BBBB
D00 - B3 D08 - G6
D01 - B4 D09 - G7
D02 - B5 D10 - R3
D03 - B6 D11 - R4
D04 - B7 D12 - R5
D05 - G3 D13 - R6
D06 - G4 D14 - R7
D07 - G5 D15 - x
RGB565 - 16 BIT COLOR(5R,6G,5B) ORGANIZED AS 16 BIT (HALF WORD)
RRRR.RGGG.GGGB.BBBB
D00 - B3 D08 - G5
D01 - B4 D09 - G6
D02 - B5 D10 - G7
D03 - B6 D11 - R3
D04 - B7 D12 - R4
D05 - G2 D13 - R5
D06 - G3 D14 - R6
D07 - G4 D15 - R7
RGB666 - 18 BIT COLOR (6R,6G,6B) ORGANIZED AS 32 BIT (WORD)
xxxx.xxxx.RRRR.RRxx.GGGG.GGxx.BBBB.BBxx
D00 - x D08 - x D16 - x D24 - x
D01 - x D09 - x D17 - x D25 - x
D02 - B0 D10 - G0 D18 - R0 D26 - x
D03 - B1 D11 - G1 D19 - R1 D27 - x
D04 - B2 D12 - G2 D20 - R2 D28 - x
D05 - B3 D13 - G3 D21 - R3 D29 - x
D06 - B4 D14 - G4 D22 - R4 D30 - x
D07 - B5 D15 - G5 D23 - R5 D31 - x
RGB888 - 24 BIT COLOR (8R,8G,8B) ORGANIZED AS 32 BIT (WORD)
xxxx.xxxx.RRRR.RRRR.GGGG.GGGG.BBBB.BBBB
D00 - B0 D08 - G0 D16 - R0 D24 - x
D01 - B1 D09 - G1 D17 - R1 D25 - x
D02 - B2 D10 - G2 D18 - R2 D26 - x
D03 - B3 D11 - G3 D19 - R3 D27 - x
D04 - B4 D12 - G4 D20 - R4 D28 - x
D05 - B5 D13 - G5 D21 - R5 D29 - x
D06 - B6 D14 - G6 D22 - R6 D30 - x
D07 - B7 D15 - G7 D23 - R7 D31 - x