i.MXRT 1010 How to execute code from RAM

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

i.MXRT 1010 How to execute code from RAM

跳至解决方案
8,248 次查看
george_phang
Contributor I

Dear NXP Team,

I'm going to try put code running on RAM (not in external SPI) in Keil project,

but seem something Keil setting problem and unable build success.

 

Could you provide some example or teach me how to configure Keil setting? 

0 项奖励
回复
1 解答
8,227 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thanks for your reply.
Sorry, I forgot to attach the file, so please check it now.
And you can learn more details by open the demo projects in the SDK library

Attachment.jpg
Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

在原帖中查看解决方案

7 回复数
8,221 次查看
george_phang
Contributor I

Hi,

 

Thanks your reply soon, I will test it right now.

So when I select to debug project, is that no need to download, just press start debug session? 

0 项奖励
回复
8,207 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi,
1) Is that no need to download, just press start to debug session?
-- Yes.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复
8,201 次查看
george_phang
Contributor I

Hi Jeremyzhou,

 Thanks you so much.

It's work.

0 项奖励
回复
8,243 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
1) Could you provide some examples or teach me how to configure Keil setting?
-- Per the attachment, you can choose the flexspi_nor_polling_transfer_debug option to put code running on RAM.
Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复
8,235 次查看
george_phang
Contributor I

Hi, 

 

 R1. Per the attachment, you can choose the flexspi_nor_polling_transfer_debug option to put code running on RAM.

- I still not understand what I do in Keil project "flexspi_nor_polling_transfer"'s debug option.

0 项奖励
回复
8,228 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thanks for your reply.
Sorry, I forgot to attach the file, so please check it now.
And you can learn more details by open the demo projects in the SDK library

Attachment.jpg
Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

8,237 次查看
george_phang
Contributor I

Hi Jeremyzhou,

 

Thanks your reply, I would like to test attached Keil mdk project and run in RAM.

Could you help me to modify option?

 

Thanks a lots.

 

 

0 项奖励
回复