i.MX RT1170 ADC input design

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX RT1170 ADC input design

1,153件の閲覧回数
TCL_1
Contributor II

Hi,

I'm designing a MIMXRT1175DVMAA based Board,  and I want to know if it is ok to have no voltage follower buffer in front of the ADC input.

As show in figure below, the acceptable maximum Ras(external analog source resistance) is 5 KOhm, does this mean the SOC internal input impedance (pointed below) is 5M Ohm around? Therefore, if a <5K Ohm analog source without buffer ok for low accuracy required ADC design?

TCL_1_0-1624003421828.png

 

thanks in advance!

Tyrone

 

0 件の賞賛
返信
0 返答(返信)