i.MX RT list of supported HyperFlash devices (octal flash)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX RT list of supported HyperFlash devices (octal flash)

Jump to solution
3,626 Views
nickwallis
Senior Contributor I

Hi,

Please can you share a list of i.MX RT supported HyperFlash devices (octal flash)?

thanks

-Nick

0 Kudos
Reply
1 Solution
3,609 Views
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thanks for your reply.
1) Which document is this table from?
-- The table is from the AN12107.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
6 Replies
3,262 Views
tfborth
Contributor I

Hi, is MX66UM1G45G also compatible? I'm looking for a 1Gb memory but it's seems that there is no one avaliable at Table 9...

0 Kudos
Reply
3,238 Views
jeremyzhou
NXP Employee
NXP Employee

Hi @tfborth ,

1) is MX66UM1G45G also compatible?

-- Yes.

BR,

Jeremy

3,222 Views
tfborth
Contributor I

Hi, thanks!

0 Kudos
Reply
3,620 Views
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
1) Please can you share a list of i.MX RT supported HyperFlash devices (octal flash)?
-- Please refer to the below figure, moreover, it's available to select the compatible octal flash for design.

jeremyzhou_0-1645521365934.png

Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply
3,616 Views
nickwallis
Senior Contributor I

thanks @jeremyzhou 

Which document is this table from?

I looked in AN12107 and whilst table 9 is referenced in the revision history, there is no table 9 in the actual document?

-Nick

0 Kudos
Reply
3,610 Views
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thanks for your reply.
1) Which document is this table from?
-- The table is from the AN12107.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply