hyper flash cannot erase/program

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

hyper flash cannot erase/program

ソリューションへジャンプ
1,888件の閲覧回数
Jay_Lin
Contributor I

Hi, the flash I use is S26KS256S. I use the upper half of the flash memory space for the second bootloader (0x60000000~0x60040000) and the remaining space for my applications.

I referred to the AN12604 manual, transplanted the "polling_transfer" example in the SDK "SDK_2_14_0_EVKB-IMXRT1050", transplanted the hyperflash operation related functions into my software and placed it in SRAM.

When I used debug to check the action of the second bootloader operating hyperflash, I discovered a strange phenomenon.

1) If I use free run, the program will crash when executing flexspi_nor_flash_erase_sector; after pausing debugging, the program will get stuck in the MCUboot.

Jay_Lin_0-1704347452823.png

------------------------------------------------------------------------------------------

Jay_Lin_1-1704347578429.png

------------------------------------------------------------------------------------------

 

2)If I add a breakpoint in the flexspi_nor_flash_erase_sector function, the flash erase operation can be completed successfully and the program can continue execution.

Jay_Lin_2-1704347765422.png

------------------------------------------------------------------------------------------

Jay_Lin_3-1704347804639.png

------------------------------------------------------------------------------------------

Jay_Lin_4-1704347832315.png

How to solve this problem?

Is hyperflash can erase/program it self? Are there any examples that I can refer to?

 

 

 

ラベル(1)
0 件の賞賛
返信
1 解決策
1,866件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @Jay_Lin ,

   Please note, the Hyperflash can't support the RWW function.

   So, your flash  operation API , eg, flexspi_nor_flash_erase_sector, program related flash file need to copy to the internal RAM.

  You can refer to project:

SDK_2_14_0_EVKB-IMXRT1050\boards\evkbimxrt1050\driver_examples\flexspi\hyper_flash\polling_transfer

  in the ld file, you can find, the flash file is copy to the internal RAM.

You also need to do it like that, then you should make it works.

 

Wish it helps you!

Best Regards,

kerry

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,867件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @Jay_Lin ,

   Please note, the Hyperflash can't support the RWW function.

   So, your flash  operation API , eg, flexspi_nor_flash_erase_sector, program related flash file need to copy to the internal RAM.

  You can refer to project:

SDK_2_14_0_EVKB-IMXRT1050\boards\evkbimxrt1050\driver_examples\flexspi\hyper_flash\polling_transfer

  in the ld file, you can find, the flash file is copy to the internal RAM.

You also need to do it like that, then you should make it works.

 

Wish it helps you!

Best Regards,

kerry

0 件の賞賛
返信