how enable cpp in imxrt1064

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

how enable cpp in imxrt1064

2,064件の閲覧回数
steve22
Contributor I

Hi all,

im new to embedded programming, and happen to be working with imxrt1064. I have a need to write cpp project files and compile. currently the project is in c, and i have a cmake file inside the project folder too. any idea what do i need to do to enable cpp? i saw a fsl_flexispi_nor_boot.c, but not sure how do i use it. Your input will be greatly appreciated, thank you! 

0 件の賞賛
返信
2 返答(返信)

2,052件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi,

Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
To provide the fastest possible support, I'd highly recommend you refer to the post to create a C++ project demo.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信

2,040件の閲覧回数
steve22
Contributor I

Hi Jeremy, 

the issue has been resolved. thank you. (:

0 件の賞賛
返信