how can i get the Code Signing Tool for rt1050's flashloader?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

how can i get the Code Signing Tool for rt1050's flashloader?

2,170件の閲覧回数
luwp
Contributor I

the document for flashloader said :

    The cst is a command-line host program used to generate certificates, image signatures, and encrypt images for i.MX MCU Boot ROM.

   note:

           These applications are released as part of Flashloader release package available on www.nxp.com/KBOOT. They are available in the <install_dir>/bin/Tools folder of the release package

but i download the flashloader's rar, can't found the tool, where can i get the  Code Signing Tool (for rt1050 flashloader)

ラベル(1)
0 件の賞賛
返信
1 返信

1,890件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

  refer to the following:

https://community.nxp.com/message/1000617 


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信