flexspi XIP mode write ability

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

flexspi XIP mode write ability

1,248 次查看
Mr-Bossman
Contributor II

Hello world!

When booting fro psram in XIP mode it seems I can't write to separate regions of the psram chip. This is unfortunate because I was hoping to use the psram+flexspi as RWX ram like the SEMC or OCRAM, but it seems to be only RX. Is this an expected result or am I configuring something wrong. I am booting the IMXRT1060-evk from SD-card at the moment and copying the program binary to the psram. 

标签 (2)
标记 (2)
0 项奖励
回复
1 回复

1,242 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
1) Is this an expected result or am I configuring something wrong?
-- In my opinion, it's impossible to implement Read While Write(RWW) on PSRAM.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复