flashing the example code on to the RAM

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

flashing the example code on to the RAM

3,231件の閲覧回数
nsnmaniram
Contributor III

hi,

is there a possibility to flash a example code on to the RAM using MCUxpresso IDE on IMXRT1050-EVKB board?

0 件の賞賛
返信
2 返答(返信)

3,080件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi maniram nagothi,

Thank you for your interest in NXP Semiconductor products and
for the opportunity to serve you.
To provide the fastest possible support, I'd highly recommend you to refers to the Building and Debugging Projects for RAM section in the attachment.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信

3,080件の閲覧回数
nsnmaniram
Contributor III

can you please provide the attachment?

0 件の賞賛
返信