firmware_swap example for imX RT1060

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

firmware_swap example for imX RT1060

Jump to solution
1,046 Views
fmabrouk
Contributor III

I need source code for this application. I dont see it in the SDK. Can I have a copy of this source code?

SW\src\boards\evkmimxrt1060\use_case\firmware_swap\.

Thanks

0 Kudos
Reply
1 Solution
1,040 Views
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
To provide the fastest possible support, I'd highly recommend you to refer to the application note which introduces how to use the flash
remapping function and the attached code is the related source code.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

 

View solution in original post

0 Kudos
Reply
1 Reply
1,041 Views
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
To provide the fastest possible support, I'd highly recommend you to refer to the application note which introduces how to use the flash
remapping function and the attached code is the related source code.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

 

0 Kudos
Reply