Hi @felix1 ,
The demo use high speed mode by default. Here is some suggestion.
No need at MCU side, baudrate is set by PC side tool.
Be noted, for USB CDC, the phisical cannel is USB port, not real UART port, the baudrate in fact does not represent the real bandwidth for communication. Even with baudrate set as 115200, I can acually get 294Mbps bandwidth like I state before.
Unless your application case is a USB-UART bridge, you need to pass the data you get from USB port to a real UART port, you in fact do not need to care much about the baudrate.
If you just use a CDC class to communicate with a PC, you in fact can ignore this parameter. USB always works at 480MHz fixed baudrate, not configurable.
Regards,
Jing