dsp code compilation error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

dsp code compilation error

3,417件の閲覧回数
zhangyin
Contributor I

Compile error on xplorer tool.

Is it a license problem and how to solve it?


Details:

Feature: XTENSA_XCC_TIE
License path: /media/ubuntu/work/work_zhangyin/s6lm_demo/iMXRT600SDK.lic:/opt/xtensa/XtDevTools/install/tools/RI-2019.1-linux/XtensaTools/Tools/lic/license.dat:
make[2]: Leaving directory '/media/ubuntu/work/work_zhangyin/s6lm_demo/SDK_2.7.0_EVK-MIMXRT685/boards/evkmimxrt685/dsp_examples/xaf_demo/dsp/xtensa/bin/nxp_rt600_RI2019_newlib/Debug/MIMXRT685S'
FLEXnet Licensing error:-5,357

......

make[2]: *** [Makefile:43: system_MIMXRT685S_dsp.o] Error 2

Import project: /SDK_2.7.0_EVK-MIMXRT685/boards/evkmimxrt685/dsp_examples/xaf_demo/dsp

0 件の賞賛
返信
2 返答(返信)

2,741件の閲覧回数
Lennart_R
Contributor I

Hello Sabina,

I got the same error.

The error came suddenly, the compile process did worked.

License checkout failed: No such feature exists.

Feature: XTENSA_XCC_TIE

License path: /home/Documents/xtensa_workspace/iMXRT600SDK.lic:/home/xtensa/XtDevTools/install/tools/RI-2020.5-linux/XtensaTools/Tools/lic/license.dat:

FlexNet Licensing error:-5,357

 

Reinstallation of the Xtensa Xplorer with Getting Started guide does not work.

I tried license file with LAN and WLAN MAC adress.

Best Regards,

Lennart

0 件の賞賛
返信

3,332件の閲覧回数
Sabina_Bruce
NXP Employee
NXP Employee

Hello Yin,

Hope you are doing well.

could you please confirm if you have followed all the steps in the Getting Started from section 2.7. Here it describes how to get the licenses and download them properly. 

If you are using Ubuntu you may follow the lines that say for linux. 

Please let me know if this was done.

Best Regards,

Sabina

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

----------------------------------------------------------------------------------------------------------------------- 

0 件の賞賛
返信