dcp hash context alignment

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

dcp hash context alignment

1,331件の閲覧回数
michalhojsik
Contributor II

Hi.

I have a question related to the DCP driver from SDK2.8.2 (SDK_2.8.2_EVK-MIMXRT1060\devices\MIMXRT1062\drivers\fsl_dcp.c).

The function DCP_HASH_Update(...) calls dcp_hash_check_context(...), which (with DCP_USE_DCACHE=1) checks that the input hash context is 32-byte aligned.

I would like to ask: Why is this check performed?

As far as I understand the documentation (i.MX RT 1050 security reference manual, Rev. 1, 04/2018, section 7.4.6 DCP context buffer pointer), there isn't any requirement for the context alignment. It only states, that it should be word-aligned for optimal performance. There is no requirement for 32-byte alignment.

Thank you.

Regards,

Michal

0 件の賞賛
返信
1 返信

1,313件の閲覧回数
FelipeGarcia
NXP Employee
NXP Employee

Hello Michal,

This is a DCACHE limitation. As you can see in the following application note, the buffer address should be L1 cache line size aligned (32 bytes in i.MXRT). Therefore, when using DCACHE 32-byte alignment is required.

https://www.nxp.com/docs/en/application-note/AN12042.pdf

Best regards,

Felipe

0 件の賞賛
返信