cache

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

cache

2,206 次查看
zhangyanming
Contributor I

Lately, i use i.MX RT1052 to develpe a product, i use cache to improve performance.But when i use the speed_test() function to test the cache performance,the code is executed in ITCM,i find that when i enable D-cache with the adram (0x80000000,2MB)memory default configuration cacheable/WT(no WA),the speed is the faster than i disable the cache.According to my understanding,WT is a write updates both the cache and the external memory system,enable and disable the cache does not affect data access speed,so why?when i enable the D-cache,i configure the adram (0x80000000,2MB)memory cache/WB(no WA),i find the cache/WT(no WA) and cache/WB(no WA) speed is same.so why? 

uint32_t AudioInData = 0;
void speed_test(void)
{
      uint32_t i = 0 , j = 0;
      for(i=0;i<30000;i++)
      {
            for(j=0;j<30000;j++)
            {
                  AudioInData += 0xA5A5;
            }
      }
}

,

0 项奖励
回复
1 回复

2,102 次查看
Yuri
NXP Employee
NXP Employee

Hello,

 

  Do You use the recent SDK (2.4.2) for i.MX RT1050?

Welcome | MCUXpresso SDK Builder 

 

  Use function BOARD_ConfigMPU() in file board.c for memory configuring.

Have a great day,

Yuri

 

------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer

button. Thank you!

0 项奖励
回复